LTE TDD

Cell Parameters Downlink (Advanced TDD Downlink)

For Waveform Playback (ARB) capability.

This topic describes the settings of the Downlink > Cell Parameters node for an Advanced TDD Downlink carrier.

Cell ID

Physical Layer Cell ID Group

Physical Layer Cell ID Sector

Total Number of Antennas

Antenna Port

System Bandwidth

Total Number of Resource Blocks

Total Number of Occupied Subcarriers

Subcarrier Spacing

Cyclic Prefix

Number of Subcarriers per RB

Number of Symbols per RB

Antenna Spacing (Wavelength)

Power Definition Type

Reference Signal Transmit Power (RSTP)

OFDM Symbol Transmit Power (OSTP)

Cell ID

Enter a value for Cell ID. The software uses this value to set the Physical Layer Cell ID Group and Physical Layer Cell ID Sector cells using:

Cell ID = (3 × Physical Cell ID Group) + Physical Cell ID Sector

See 3GPP TS 36.211 for more information.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CIDentity <integer>

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CIDentity?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:CIDentity 0

:RADio:LTETdd:WAVeform:CCARrier:DLINk:CIDentity?

Dependencies

Default 0 with Auto Carrier Aggregation Configuration set to Off; same as the CC index number with Auto Carrier Aggregation Configuration set to On.

Controls Physical Layer Cell ID Group/Sector (Cell ID = 3 × Group + Sector).

Preset

1

State Saved

Yes

Min

0

Max

503

Initial S/W Revision

A.20.01

Physical Layer Cell ID Group

Query only

Displays the Physical Layer Cell ID Group. This value is set by software based on Cell ID.

Formula: Cell ID = (3 x Physical Cell ID Group) + Physical Cell ID Sector.

Ref: 3GPP TS 36.211.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PLCid:GRP?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:DLINk:PLCid:GRP?

Range

0 to 167 (related to cell ID) 

Couplings

Coupled to Cell ID

Preset

0

State Saved

Yes

Min

0

Max

167

Initial S/W Revision

A.20.01

Physical Layer Cell ID Sector

Query only

Displays the Physical Layer Cell ID Sector. This value is set by software based on Cell ID.

Formula: Cell ID = (3 x Physical Cell ID Group) + Physical Cell ID Sector.

Ref: 3GPP TS 36.211.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PLCid:SECT?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:DLINk:PLCid:SECT?

Range

0 | 1 | 2

Couplings

Coupled to Cell ID

Preset

1

State Saved

Yes

Min

0

Max

2

Initial S/W Revision

A.20.01

Total Number of Antennas

In multi-antenna configurations, specify the total number of antennas used for the downlink transmission.

For multiple signal generator configurations, set the Channel State parameter in the Fading section of the Carrier node to On to make this cell active. When the channel state is off, you must change the number of signal generators (for example, Quick Setup Mx1, Mx2, Mx4, Mx8) to change the number of BS antennas.

This parameter indicates the total number of physical antenna port configuration used for downlink transmission in this cell.

Total Number of Antennas and Number of CRS Antenna Ports determine the resource elements that are reserved for Cell Specific reference signals.

Refer to 3GPP TS 36.211 and 36.311.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:APORts:COUNt 1|2|4|8

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:APORts:COUNt?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:APORts:COUNt 1

:RADio:LTETdd:WAVeform:CCARrier:DLINk:APORts:COUNt?

Couplings

Coupled to Number of CRS Antenna Ports (CRS Antenna Ports must be ≤ Total Number of Antennas).

  • When Total Number of Antennas is 1, Number of CRS Antenna Ports is One Port

  • When Total Number of Antennas is 2, Number of CRS Antenna Ports is Two Ports

  • When Total Number of Antennas is 4, Number of CRS Antenna Ports is Four Ports

  • When Total Number of Antennas is 8, Number of CRS Antenna Ports is Four Ports

Preset

1

State Saved

Yes

Min

1

Max

8

Initial S/W Revision

A.20.01

Antenna Port

Sets the physical antenna port for transmitting downlink signals.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:APORt <integer>

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:APORt?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:DLINk:APORt 0

RADio:LTETdd:WAVeform:CCARrier:DLINk:APORt?

Notes

Available selections are determined by Total Number of Antennas.

  • When Total Number of Antennas is 1, Antenna Port range is 0

  • When Total Number of Antennas is 2, Antenna Port range is 0,1

  • When Total Number of Antennas is 4, Antenna Port range is 0,1,2,3

  • When Total Number of Antennas is 8, Antenna Port range is 0,1,2,3,4,5,6,7

Preset

PORT0

State Saved

Yes

Min

N/A

Max

N/A

Initial S/W Revision

A.20.1

System Bandwidth

Sets system bandwidth. Based on the selected System Bandwidth, the Total Number of Resource Blocks and Total Number of Occupied Sub-carriers are automatically adjusted. These are automatically reconfigured when system bandwidth changes.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:BANDwidth
F1_4M|F3M|F5M|F10M|F15M|F20M

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:BANDwidth?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:BANDwidth B10M

:RADio:LTETdd:WAVeform:CCARrier:DLINk:BANDwidth?

Preset

F10M

State Saved

Yes

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Total Number of Resource Blocks

The value in this cell is set by the software based on the System Bandwidth setting.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:RB:COUNt?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:RB:COUNt?

Notes

Computed by software from System Bandwidth.

Preset

50

State Saved

No

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Total Number of Occupied Subcarriers

The value in this cell is set by the software based on the System Bandwidth setting. The center subcarrier is not used for downlink transmission, so the number of transmitted subcarriers is one less than the number of occupied subcarriers.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:SCARrier:COUNt?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:SCARrier:COUNt?

Notes

Computed by software from System Bandwidth.

Preset

600

State Saved

No

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Subcarrier Spacing

Query only

Displays the subcarrier spacing.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:SCSPacing?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:SCSPacing?

Notes

Computed by software (Default 15 kHz).

Preset

F15K

State Saved

No

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Cyclic Prefix

Selects a Normal or Extended cyclic prefix. The software sets the Number of Symbols for Resource Block based on the cyclic prefix selection.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CP NORMal|EXTended

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CP?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:CP NORMal

:RADio:LTETdd:WAVeform:CCARrier:DLINk:CP?

Dependencies

For Basic, Advanced UL, and Advanced DL LTE-A TDD when Auto Carrier Aggregation Configuration is set to On, this setting is read-only for the secondary cells that has the same value as the primary cell.

Controls Number of Symbols per RB.

Preset

NORMal

State Saved

Yes

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Number of Subcarriers per RB

Query only

Displays the number of consecutive subcarriers in a resource block.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:RB:SCARrier:COUNt?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:RB:SCARrier:COUNt?

Notes

Computed by software (Default 12).

Preset

12

State Saved

No

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Number of Symbols per RB

Query only

Displays the number of consecutive OFDM symbols in a slot.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:RB:SYMBol:COUNt?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:RB:SYMBol:COUNt?

Dependencies

Computed by software

  • Default 7 for Normal CP

  • Default 6 for Extended CP

Preset

7

State Saved

No

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Antenna Spacing (Wavelength)

Enter a value that specifies the distance between the antennas. The value is specified in wavelength units of the center frequency for the corresponding Component Carrier.

Use this setting when generating a beamforming signal.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:ASPacing <double>

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:ASPacing?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:ASPacing 0.5

:RADio:LTETdd:WAVeform:CCARrier:DLINk:ASPacing?

Preset

0.5

State Saved

Yes

Min

0.00

Max

100

Initial S/W Revision

A.20.01

Power Definition Type

Selects the power definition type for the primary cell.

The power definition type for secondary cells is automatically set to the same type as the primary cell and set as read-only.

In multiple carrier case, the Power Definition Type parameter in each carrier should be same.

If uplink and downlink carriers are mixed as multiple carriers, correct RSTP calculation is not available.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PDType TPOW|RSTP

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:PDType?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:PDType TPOW

:RADio:LTETdd:WAVeform:CCARrier:DLINk:PDType?

Notes

All carriers in an aggregation must use the same Power Definition Type.

Dependencies

Controls the read-only state of RSTP and Power.

Preset

TPOW

State Saved

Yes

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Reference Signal Transmit Power (RSTP)

Sets the Reference Signal Transmit Power. Automatically calculated from Amplitude, Power, and carrier signal settings.

Ref: 3GPP TS 36.141.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:RSTP <rel-ampl>

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:RSTP?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:RSTP -40.79

:RADio:LTETdd:WAVeform:CCARrier:DLINk:RSTP?

Notes

Value is in dBm.

Dependencies

In case Power Definition Type is Total Power, RSTP is automatically calculated by the software and the value is read-only,

In case Power Definition Type is RSTP, the value is settable.

Preset

-40.79

State Saved

Yes

Min

-144

Max

-15

Initial S/W Revision

A.20.01

OFDM Symbol Transmit Power (OSTP)

Query only

Displays the Downlink OFDM Symbol Transmit Power, in dBm. This parameter is set by the software from Power Definition Type and related power settings.

For detailed information about OSTP, refer to 3GPP TS 36.141.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:OSTP?

SCPI Example

:RADio:LTETdd:WAVeform:CCARrier:DLINk:OSTP?

Preset

-13.01

State Saved

No

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Carrier Advanced TDD Downlink ARB

Welcome to LTE TDD